Solution
Turkey Weighing
A customer wants a weighing system to help them determine a specific weight for their turkeys for the holidays.
A customer wants a weighing system to help them determine a specific weight for their turkeys for the holidays. They need a weighing system that will ensure accurate weight measurements to keep their birds at their weight in order to sell to supermarkets. They also need a system that will be able to undergo harsh conditions and unusual temperatures.
Interface’s SPI Low Capacity Platform Scale Load Cell is able to undergo strained temperatures and transmits highly accurate results. A plate can be put on top of the SPI, and then a turkey can be weighed on top of the plate. Data results can be displayed on the 480 Bidirectional Digital Weight Indicator.
The customer is able to weigh their turkeys, and maintain their weight through the accurate results from Interface’s SPI Low Capacity Platform Scale Load Cell.
Notifications